FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > CC-Link
FAQ
CC-Link
I used the CC-Link option FR-A7NC to set Pr.542 (Station number), and set Pr.340 (Communication startup mode selection) to "1".
When I powered on the inverter, it entered the CC-Link NET mode.
1. What happens with external terminals such as high speed in CC-Link operation?
2. What happens with the external reset terminal?
When I powered on the inverter, it entered the CC-Link NET mode.
1. What happens with external terminals such as high speed in CC-Link operation?
2. What happens with the external reset terminal?
- Category :
Answer
1. It depends on how Pr.338 (Communication operation command source) and Pr.339 (Communication speed command source) are set.
2. The external terminal reset is effective as the external signal without regard to the setting of Pr.338 and Pr.339. During CC-Link operation, error reset is available by turning ON RY1A (Error reset request flag).
This error reset request flag turns OFF after reset.
Run the reset as necessary using the instruction code even when no error occurs.
2. The external terminal reset is effective as the external signal without regard to the setting of Pr.338 and Pr.339. During CC-Link operation, error reset is available by turning ON RY1A (Error reset request flag).
This error reset request flag turns OFF after reset.
Run the reset as necessary using the instruction code even when no error occurs.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700