FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Frequency setting
FAQ
Frequency setting
I want to use the "RUN" key on the operation panel to start the inverter and use the setting dial to set the frequency.
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
If Pr.79 (Operation mode) is set to "0" (PU/EXT switching mode), press the PU/EXT button on the operation panel to turn on the PU LED.
Turn the setting dial to set the frequency and press the "SET" key to accept it.
If Pr.79 (Operation mode) is set to "1" (PU operation mode), the PU LED is already turned on. Use the setting dial to set the frequency.
Turn the setting dial to set the frequency and press the "SET" key to accept it.
If Pr.79 (Operation mode) is set to "1" (PU operation mode), the PU LED is already turned on. Use the setting dial to set the frequency.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700