Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21865
  • Release Date : 2018/08/22 16:29
  • Print

Terminal FM

I want to use the ammeter connected to the terminal FM so that the output current monitor 10 A becomes the full scale.
Category : 

Answer

Set Pr.56 (Current monitor reference) to "10A".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries