FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Frequency setting
FAQ
Frequency setting
I input the start signal from an external terminal and the frequency setting signal from the CC-Link, but the setting of the running frequency cannot be written.
- Category :
Answer
Set Pr.338 (Operation command source) to "1" (external terminal).
Set Pr.339 (Speed command source) to "0" (communication).
Check the setting of Pr.79 for operation mode and Pr.340 (Communication startup mode selection).
To set the running frequency, set the frequency at the address "RWwn + 1" in 0.01 units and then turn ON the frequency setting command (RYD).
Set Pr.339 (Speed command source) to "0" (communication).
Check the setting of Pr.79 for operation mode and Pr.340 (Communication startup mode selection).
To set the running frequency, set the frequency at the address "RWwn + 1" in 0.01 units and then turn ON the frequency setting command (RYD).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700