FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > CC-Link
FAQ
CC-Link
I want to install the CC-Link option to the inverter that I have been using and monitor the output current value.
Does the operation method change?
Does the operation method change?
- Category :
Answer
The way to monitor the output current and read parameters via CC-Link is identical in all operation modes.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700