Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21885
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

I cannot find explanation on how to monitor power in the Instruction Manual of the FR-A7NC. Is it possible?
What is the unit of power output?
Category : 

Answer

You can select from the output power (in 0.01 kW units) and cumulative energy (in 1 kWh/0.01 kWh units).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries