FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > CC-Link
FAQ
CC-Link
I want to configure the inverter via communication using the FR-A7NC.
Is it no longer necessary to wire the external terminals of the inverter if I use this option?
Is it no longer necessary to wire the external terminals of the inverter if I use this option?
- Category :
Answer
When configuring the inverter via communication such as CC-Link, some signals still requires to be input from the external terminals.
(Terminal OH: External thermal relay input and others)
If you need any of these signals, you still need cabling the external terminals.
(Terminal OH: External thermal relay input and others)
If you need any of these signals, you still need cabling the external terminals.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700