FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > CC-Link
FAQ
CC-Link
I use multiple inverters in CC-Link communication, and the "L.RUN" LED on the optional board does not turn on.
How can I check for the cause?
How can I check for the cause?
- Category :
Answer
Check if the CC-Link wires are short-circuited and/or station numbers are duplicated.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700