FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > CC-Link
FAQ
CC-Link
Should I purchase the FR-A7NC option to implement CC-Link communication?
- Category :
Answer
Purchase the FR-A7NC if you are using the option with the FR-A700 or FR-F700P (F700).
Purchase the FR-A7NC E kit if you are using the option with the FR-E700.
Purchase the FR-A7NC E kit if you are using the option with the FR-E700.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700