FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Frequency setting
FAQ
Frequency setting
I set the maximum frequency to 85 Hz, but the frequency does not increase higher than 63.1 Hz.
I send the frequency command from the frequency setting potentiometer connected to the terminals 10, 2, and 5.
I send the frequency command from the frequency setting potentiometer connected to the terminals 10, 2, and 5.
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
Since Pr.125 (Terminal 2 frequency setting gain frequency) is initially set to 60 Hz, change it to 85 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700