FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Frequency setting
FAQ
Frequency setting
If I set up an external frequency setting potentiometer and connect to the terminals 10, 2, and 5, can I use this frequency setting potentiometer to command the reversible operation, forward and reverse rotations?
- Category :
Answer
You can do so by setting Pr.73 to "10" or "11". (For A700/F700 (P), supply negative input to the terminal 1.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ