FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Frequency setting
FAQ
Frequency setting
I set an externally connected potentiometer (frequency setting potentiometer) for manual operation and connected it to the terminals 10, 2, and 5. In addition, I connected an external source to the terminals 4 and 5 to supply voltage input for automatic operation.
Now I want to switch these manual and automatic operations.
Now I want to switch these manual and automatic operations.
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
You can do so by assigning the terminal AU.
Assign the terminal AU to an unused terminal.
(For example, when assigning AU to the terminal RL, set Pr.180 = 4.)
By providing a switch between the terminals AU and SD, you can select the automatic operation by short-circuiting the switch and the manual operation by opening it.
Assign the terminal AU to an unused terminal.
(For example, when assigning AU to the terminal RL, set Pr.180 = 4.)
By providing a switch between the terminals AU and SD, you can select the automatic operation by short-circuiting the switch and the manual operation by opening it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700