Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21935
  • Release Date : 2018/08/22 16:30
  • Print

Using a higher grade power factor improving reactor

Can I use the FR-BEL-1.5K instead of the FR-BEL-750)? Does the greater also serve for the lesser?
Category : 

Answer

Using a reactor under a load lighter than the rated capacity slightly spoils its effect in improving the power factor.
Therefore, you should use a reactor with the similar capacity to that of the motor.
Product Name
Inverter, magnet motor drive
Product Category
Power factor improving reactor
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries