FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Applied motor selection
FAQ
Applied motor selection
Pr.71 (Applied motor selection) is set according to the load connected to the inverter. What happens if, for example, I choose the standard motor while the Mitsubishi constant-torque motor is connected?
- Category :
Answer
As the motor operates with the electronic thermal O/L relay characteristics for the standard motor, the thermal error occurs if the motor continuously operates at low speed operation under 100% load.
It means that you are using the constant-torque motor at lower performance. Select the correct motor type with Pr.71.
It means that you are using the constant-torque motor at lower performance. Select the correct motor type with Pr.71.
- Product Name
- Inverter, magnet motor drive
- Series
- Others