FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Using built-in potentiometer and multi-speed together
FAQ
Using built-in potentiometer and multi-speed together
Can I use both the built-in potentiometer and multi-speed signal for 2-speed operation?
- Category :
Answer
Yes. Set Pr.79 = 3. (Input the start signal from an external source.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500