Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21977
  • Release Date : 2018/08/22 16:30
  • Print

Fault output contact rating

The rating of the fault output terminals A-C and B-C is defined as 30 VDC 0.3 A, are they capable of a micro load of 5 VDC±5% and 10 mA?
Category : 

Answer

They are capable of a load of 5 VDC±5% and 10 mA.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries