Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21988
  • Release Date : 2018/08/22 16:30
  • Print

Motor heat generation

I use the MM-CF352 (rated current 12.5 A) at around 4 A. (24-hour continuous operation)
The surface temperature is approximately 70 deg C. Is this OK?
Category : 

Answer

The surface temperature of approximately 70?C is OK.
The following shows the MM-CF352 frame temperature for reference.
(Actual temperature rise depends on how the motor is attached.)
- Rated speed (2000 r/min), Under rated load: Around 60 degrees
- Rated speed (2000 r/min), Under no load: Around 30 degrees
If you install the motor where people may touch it, attach a cover to it to prevent the motor from being touched.
Product Name
Inverter, magnet motor drive
Product Category
Motor
Series
Magnetic motor drive

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries