Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22015
  • Release Date : 2018/08/22 16:30
  • Print

Single-phase power supply drive

I am considering to use a single-phase 200 V power supply with the inverter. If I use a three-phase 200 V, 3.7 kW standard induction motor, should I choose an inverter with the capacity that is two times the motor rated capacity?
Can I use the inverter?
Category : 

Answer

For a single-phase 200 V power supply, you can use the FR-E520S series for up to 0.75 kW motor.
If you use the three-phase 200 V power supply inverter with a single-phase 200 V power supply, you can use an inverter of 3.7 kW or lower by reducing the inverter's current capacity to 1/3.
Product Name
Inverter, magnet motor drive
Series
Others

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries