Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22030
  • Release Date : 2018/08/22 16:30
  • Print

Operation panel

I want to remove the operation panel from the FR-E520-5.5K and attach it to a machine. What are the mounting dimensions?
Is the FR-E5P necessary for this purpose?
Can I use a commercial straight LAN cable for connection?
Category : 

Answer

Be sure to use the FR-E5P to mount the operation panel.
This is because the board is bare on the back of the operation panel and a dedicated connector is required for cable connection.
You can use a commercial straight LAN cable for connection.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries