FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > Installation clearance of inverters
FAQ
Installation clearance of inverters
I am planning to install two inverters next to each other.
How long should the FR-520-5.5K and FR-520-3.7K be apart from each other?
How long should the FR-520-5.5K and FR-520-3.7K be apart from each other?
- Category :
Answer
Keep 1 cm or more of clearance for 3.7 K or smaller, and 5 cm or more for 5.5 K or larger.
If the clearance is too small, the cooling effect is lowered. Secure 5 cm or more clearance between inverters.
If the clearance is too small, the cooling effect is lowered. Secure 5 cm or more clearance between inverters.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500