Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22054
  • Release Date : 2018/08/22 16:30
  • Print

Pulse train output of terminal FM

I utilize the pulse train output from the inverter's terminal FM to display the rotations per minute display with GOT.
The full-scale value should be 1440 pulses/sec, however, the display value differs in no load, full load, and overload. What is the possible cause?
Category : 

Answer

Under Advanced magnetic flux vector control, the output frequency varies due to slip compensation. This may cause the output frequency monitor value to change and the pulse count varies accordingly.
Also, under V/F control, the output frequency can change due to stall prevention operation and the output pulse count can decrease.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries