FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500 > Operation command terminal switching
FAQ
Operation command terminal switching
While the FR-E520 is rotating in the forward direction with the terminal STF turned ON, how does the inverter operate if it is switched to STR (with STF turned OFF)?
- Category :
Answer
It rotates in the forward direction while STF is ON.
And then, when STR is turned ON and STF is turned OFF, the inverter decelerates down to 0 Hz within the specified deceleration time. Then, it accelerates to the setting frequency in the reverse rotation within the specified acceleration time.
And then, when STR is turned ON and STF is turned OFF, the inverter decelerates down to 0 Hz within the specified deceleration time. Then, it accelerates to the setting frequency in the reverse rotation within the specified acceleration time.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500