Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22072
  • Release Date : 2018/08/22 16:30
  • Print

Parameter unit display

I use the inverter to rotate a roller and want to monitor the rotations per minute of the roller on the parameter unit.
Can I switch the frequency monitor (or any other monitors) to the roller rotations per minute monitor?
Category : 

Answer

Setting Pr.37 to the machine speed at 60 Hz switches the frequency monitor to the rotations per minute monitor.
Note that the speed setting must be input in as the machine speed.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries