FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Which motors can I use with the inverter?
FAQ
Which motors can I use with the inverter?
Let me know which types of motors I can use with the inverter.
Which should I choose from various types of motors (for example, geared motors, induction motors)?
Which should I choose from various types of motors (for example, geared motors, induction motors)?
- Category :
Answer
You can use general-purpose three-phase induction motors.
You can also use geared motors if the motor itself is an induction motor.
Synchronous motors are not recommended due to possible synchronization loss.
Note that single-phase motors cannot be used.
You can also use geared motors if the motor itself is an induction motor.
Synchronous motors are not recommended due to possible synchronization loss.
Note that single-phase motors cannot be used.
- Product Name
- Inverter, magnet motor drive
- Series
- Others