Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22099
  • Release Date : 2018/08/22 16:30
  • Print

Motor rated rotations per minute

Is it possible to use a standard three-phase motor (SF-JR) 2-pole 0.4 kW and the inverter to perform high-speed rotation of 4000 to 6000 (MAX 9000)?
Category : 

Answer

The inverter is capable of output up to the maximum frequency. It is the matter of whether the motor used support high-speed operation.
In the situation you mention, it is considered to be hard for the motor to operate at that high speed.

For details, consult our technical support below.
Shinshiro plant technical telephone support Phone: 0536-25-0900
Product Name
Inverter, magnet motor drive
Series
Others

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries