Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22104
  • Release Date : 2018/08/22 16:31
  • Print

Suggestion for replacement of inverters

I want to replace the FR-Z123 with one of the current types of inverters. Which type is easy to replace the FR-Z123 from viewpoints of dimensions and parameter settings?
I also want to upgrade the Z024. Is the A024 a good candidate?
Category : 

Answer

We do not offer book type inverters. Therefore, the S500 is recommended to replace the Z123 because of its compact design. If regenerative driving matters, consider the E500.

The S500 is also recommended to replace the Z024. If regenerative driving matters, consider the E500.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-Z024, FR-Z123

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries