FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > Method for measuring a circuit over 600A (EcoMonitorPlus/Light).
FAQ
Method for measuring a circuit over 600A (EcoMonitorPlus/Light).
Instruct a method for measuring a circuit over 600A using the Energy Measuring Unit (EcoMonitorPlus/Light).
Answer
Attach a current transformer (CT) whose secondary current is 5A to the measuring point, then connect a split-type 5A current sensor (Model: EMU-CT5-A, EMU2-CT5, EMU2-CT5-4W) with the secondary side of the CT.
1. In case of EcoMonitorPlus.
1. In case of EcoMonitorPlus.
2. In case of EcoMonitorLight.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight
May I have your opinion?
Related FAQ
- Method for creating a daily/monthly report using logging data (Model: EMU4-LM).
- Extension of current sensor cable (EcoMonitorPlus/Light).
- Recommended replacement cycle for battery (EcoWebServerIII).
- As to logging period of the internal memory of the main unit.
- Simultaneous data acquisition of MODBUS RTU communication and Optional Unit.