FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to simple measuring function of the EcoMonitorPlus (Model: EMU4-BM1-MB、EMU4-HM1-MB、EMU4-A2、EMU4-VA2).
FAQ
As to simple measuring function of the EcoMonitorPlus (Model: EMU4-BM1-MB、EMU4-HM1-MB、EMU4-A2、EMU4-VA2).
How does simple measuring function of EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2) work?
Answer
The function calculates the value of each measurement element of voltage, power factor by inputting only current using setting value.
This function is used when wiring for voltage input is impossible due to installation environment or wiring condition. Refer to "user's manual detailed edition" for each unit as to details like measurement elements.
The manual is downloadable in this site.
This function is used when wiring for voltage input is impossible due to installation environment or wiring condition. Refer to "user's manual detailed edition" for each unit as to details like measurement elements.
The manual is downloadable in this site.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus
May I have your opinion?
Related FAQ
- As to settings for EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-LG1-MB, EMU4-A2, EMU4-VA2, EMU4-AX4, EMU4-PX4).
- As to timing for outputting data file into the SD memory card.
- As to Zero-Phase Current Transformer (ZCT) usable for the EcoMonitorPlus (Model: EMU4-LG1-MB).
- As to using SD memory card at multiple locations.
- As to periodic electric energy (EcoMonitorPlus/Light).