FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding the type of battery which can be used with the CPU module.
FAQ
Regarding the type of battery which can be used with the CPU module.
What is the model name of the battery that can be used with the CPU module?
Answer
FX3U-32BL can be used.
The battery is not included with the CPU module during factory shipment.
The battery can be used to increase the capacity of the latch device/label, as well as to maintain the clock data during power interruption.
The battery is not included with the CPU module during factory shipment.
The battery can be used to increase the capacity of the latch device/label, as well as to maintain the clock data during power interruption.
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, Options
- Series
- MELSEC iQ-F Series