Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 22389
  • Release Date : 2018/08/31 14:33
  • Print

F-type and V-type operating handle

What is the difference between F-type and V-type operating handle?
Category : 

Answer

Both of F-type and V-type can remotely operate a circuit breaker in the panel board and the design of 800A fame or less are unified. Features are as follows.
*F-type control handle: It is installed on a circuit breaker itself
*V-type control handle: The handle part is installed on the door side of the panel board and mechanism part is installed on circuit beaker itself. (It is suitable for cases where the depth from the panel door to the mounting surface of a circuit breaker is deep)
Product Name
External Accessories
Series
WS-V

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries