Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 22431
  • Release Date : 2018/08/31 14:33
  • Print

ACB drawout position

Which drawout positions are there for Drawout type?
Category : 

Answer

Drawout type circuit breaker can be drawn-out and insert to the cradle without taking out the connecting conductor. As ACB is drawn out, it will be "connect position" , "Test position" (main circuit is disconnected and only control circuit is connected) and "Disconnect position" (both main circuit and control circuit are disconnected)
Product Name
Low Voltage Air Circuit Breakers
Series
AE-SW

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries