Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22460
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/19 11:46
  • Print

Changing the display language of device comments with GX Works3

How can I change the display language of device comments with GX Works3?
Category : 

Answer

In the multiple comments display setting, you can set a comment title of the device comments to be set.

<Displaying the multiple comments display setting>
[View] -> [Mulitple Commnets Dispaly Setting]

<Setting procedure>
(1) Put a checkmark in "Enable Multiple Comments Dispaly".
(2) Put a checkmark in "Available" and enter a comment tile.
(3) Select comments to be displayed in the program editor or various monitor screens in "Target".
(4) Enter a comment in each row in the device comment editor.

Set device comments for each language in the device comment editor.
<Setting device comments>
[Navigation Window] -> [Device] -> [Device Comment]
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?