FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > I/O numbers of a MELSEC iQ-R series I/O combined module (RH42C4NT2P)
FAQ
I/O numbers of a MELSEC iQ-R series I/O combined module (RH42C4NT2P)
How are I/O numbers of a MELSEC iQ-R series I/O combined module (RH42C4NT2P) used?
- Category :
Answer
An input and output use a single I/O number. (This is the same as QH42P.)
When you replace a module that uses serial I/O numbers (e.g. QX41Y41P) with this module, change the I/O numbers.
When you replace a module that uses serial I/O numbers (e.g. QX41Y41P) with this module, change the I/O numbers.
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Models of batteries that can be used with MELSEC iQ-R series CPU modules
- How to change the specified connection destination of GX Works3
- Overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module is executed
- The number of times to insert and remove the extended SRAM cassette and SD memory card of a MELSEC iQ-R series CPU module
- How to display the network parameter setting window with GX Works3