Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22471
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/19 13:57
  • Print

I/O numbers of a MELSEC iQ-R series I/O combined module (RH42C4NT2P)

How are I/O numbers of a MELSEC iQ-R series I/O combined module (RH42C4NT2P) used?
Category : 

Answer

An input and output use a single I/O number. (This is the same as QH42P.)
When you replace a module that uses serial I/O numbers (e.g. QX41Y41P) with this module, change the I/O numbers.
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?