Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22475
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/19 14:42
  • Print

I/O assignment of PLC parameters with GX Works3

Where can I set the I/O assignment of PLC parameters with GX Works3?
Category : 

Answer

"PC Parameter" in GX Works2 is "Parameter" in GX Works3.
You can set the I/O assignment from "Module Configuration" or "System Parameter".

<Setting from the module configuration>
[Navigation Window] -> [Project] -> [Module Configuration]

<Setting from the system parameter>
[Navigation Window] -> [Parameter] -> [System Parameter] -> [I/O Assignment]
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries