Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22523
  • Release Date : 2018/09/03 17:28
  • Print

Battery life

How long is the battery life installed in a High-Performance model QCPU?
Category : 

Answer

It depends on the model of the CPU module, the amount of battery consumption, and the power-on time ratio.
Example) For Q06HCPU with power-on time ratio of 50%, the guaranteed value is 41,785 hours (4.77 years)

For more details, refer to the following manual.
- QCPU User's Manual (Hardware Design, Maintenance and Inspection)
-Appendix 4 Battery Life
Product Name
MELSEC-Q Series
Series
Q (Q mode)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries