Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22528
  • Release Date : 2018/09/03 17:28
  • Print

High-speed timer

How do I insert a high-speed timer into a circuit?
Category : 

Answer

Follow the procedure below to insert a high-speed timer.

- Click the Coil button on the toolbar or press the function key F7, then enter "HT[ ] K[ ]".

- Click the Application Instruction button on the toolbar or press the function key F8, then enter "OUTH T[ ] K[ ]".

- Enter "OUTH K[ ] T[ ]" using the keyboard.
Product Name
Engineering Software
Series
Software Package (GPP function)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?