Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22548
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 15:40
  • Print

Unable to select [Transfer Setup]

[Transfer Setup] on the menu is grayed out and the connection destination cannot be changed.
How can I enable the grayed out item?
Category : 

Answer

If a circuit is being monitored or a monitor window such as the device batch monitor window is open,
[Transfer Setup] on the menu is grayed out.
Select [Window] on the menu and check currently opened windows.
Stopping monitoring the circuit or closing the monitor window enables [Transfer Setup] on the menu.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries