Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22569
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/20 16:50
  • Print

USB communication driver

MX Component does not work on a Windows 7-based personal computer with an existing USB communication driver installed.
What are the possible causes?
Category : 

Answer

Is the version of MX Component compatible with Windows 7?
Update the software to the version compatible with Windows 7 and then update the driver.
For the update procedure of the driver, refer to the following technical bulletin.
- FA-A-0091: Products compatible with Windows 7 and precautions for installation
Product Name
MELSEC-Q Series
Series
Middleware

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries