Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22608
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/20 18:09
  • Print

QnA-compatible 3E frame command (0406) for the built-in Ethernet port QCPU

An error C059h is returned when I use a multiple-block batch read command (0406) for the QnA-compatible 3E frame of the MC protocol in a built-in Ethernet port QCPU. What is the remedy?
Category : 

Answer

The built-in Ethernet port QCPU is not compatible with a multiple-block batch read command (0406) of the MC protocol.
Executable commands are the following.

- Batch read: 0401
- Batch write: 1401
- Random read: 0403
- Test (random write): 1402
- Monitor registration: 0801
- Monitor: 0802
- Remote password unlock: 1630
- Remote password lock: 1631
Product Name
MELSEC-Q Series
Series
Q (Q mode)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries