Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22624
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 10:32
  • Print

Counting operation of QD62

What happens if the count value exceeds the upper limit of the 32-bit counting range of QD62/QD62E/QD62D?
Category : 

Answer

The corresponding operation depends on the counter type selected.

(1) If "Linear Counter" is selected
      If the present counter value exceeds the upper limit, an overflow error occurs.
      Counting is stopped when the error occurs.

(2) If "Ring Counter" is selected
      Counting is repetitively performed between an upper limit and a lower limit set beforehand.
      No overflow error occurs.
Product Name
MELSEC-Q Series
Series
High Speed Counter Module

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries