Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22633
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 11:28
  • Print

Battery life in the universal model QCPU

How long is the battery life installed in a universal model QCPU module?
Category : 

Answer

It depends on the model of the CPU module, the amount of battery consumption, and the power-on time ratio.

Example) For Q06UDHCPU with power-on time ratio of 50%, the guaranteed value is 43,800 hours (5.00 years).
For more details, refer to the following manual.

 - QCPU User's Manual (Hardware Design, Maintenance and Inspection) Appendix 4 Battery Life
Product Name
MELSEC-Q Series
Series
CPU

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries