Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22644
  • Release Date : 2018/09/03 17:29
  • Print

Copying programs when replacing the CPU module

Is it possible to copy programs and parameters from the control system CPU module under operation in a Q series redundant system when the standby system CPU module is replaced?
Category : 

Answer

Programs and parameters can be copied using the memory copy function.
There are the following two methods of executing the memory copy function.
- Using the memory copy function of GX Developer
- Using special relays and registers
For more details, refer to the following manual.
- QnPRHCPU User's Manual (Redundant System) Section 5.7
Product Name
MELSEC-Q Series
Series
CPU

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries