Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22685
  • Release Date : 2018/09/03 17:29
  • Print

Intelligent function module settings in GX Works2

How do I configure the setting for an intelligent function module that is not available from the module selection?
Category : 

Answer

Modules do not need setting in GX Works2 if not selectable from "Module Selection" in the "New Module" window for intelligent function module settings.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?