FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > How to increase file register capacity
FAQ
How to increase file register capacity
How do I increase file register capacity in a universal model QCPU module?
- Category :
Answer
An SRAM card can increase file register capacity.
1MB/2MB/4MB/8MB SRAM cards are available.
The numbers of file registers that can be used with a 1MB, 2MB, 4MB, and 8MB SRAM cards are 517,120, 1,041,408, 2,087,936, and 4,184,064 respectively.
For Q00UJ/Q00U/Q01UCPU, however, an SRAM card cannot be used.
1MB/2MB/4MB/8MB SRAM cards are available.
The numbers of file registers that can be used with a 1MB, 2MB, 4MB, and 8MB SRAM cards are 517,120, 1,041,408, 2,087,936, and 4,184,064 respectively.
For Q00UJ/Q00U/Q01UCPU, however, an SRAM card cannot be used.
- Product Name
- MELSEC-Q Series
- Series
- CPU