Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22689
  • Release Date : 2018/09/03 17:29
  • Print

Update timing of QD75 current feed value and machine feed value

When are the current feed value and the machine feed value of QD75P1/P2/P4/D1/D2/D4 updated?
Category : 

Answer

The values are updated at the timing described below.
- Current feed value: 1.8 ms
- Machine feed value: 56.8 ms
Product Name
MELSEC-Q Series
Series
Positioning Module

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries