FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Remedy for the division-related operation error
FAQ
Remedy for the division-related operation error
An operation error occurs when a division operation is performed. What is the remedy for the error?
- Category :
Answer
The operation error occurs when the divisor is 0.
Create a program in which a comparison operation instruction or another method executes a division instruction only when the divider is not 0 .
Create a program in which a comparison operation instruction or another method executes a division instruction only when the divider is not 0 .
- Product Name
- MELSEC-Q Series
- Series
- CPU
May I have your opinion?
Related FAQ
- Cables connected to the Ethernet port on the universal model QCPU
- Compatibility between the A series modules and Q series modules
- How to check the capacity of the file registers in use
- Specifying steps in printing data displayed in the window in GX Works2
- How to check automatically assigned devices in GX Works2