Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22720
  • Release Date : 2018/09/03 17:29
  • Print

Pulse width with which the QX42 recognizes all pulses

How wide is the pulse width with which the QX42 recognizes all pulses with the set response time? For example, when 10 ms has been set as the response time with the scan time of 10 ms, how wide is the pulse width with which the module recognizes all input pulses? 
Category : 

Answer

Maximum scan time (10 ms) + Response time (10 ms) = Pulse width with which the module recognizes all pulses (20 ms)
Product Name
MELSEC-Q Series
Series
Input Module

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries