FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > L63P compatibility with L series CPU packages
FAQ
L63P compatibility with L series CPU packages
Is it possible to purchase L63P separately to replace L61P power supply module of the L series CPU package?
- Category :
Answer
It is possible to remove L61P and use L63P.
- Product Name
- MELSEC-L Series
- Series
- L Series
May I have your opinion?
Related FAQ
- Use of a commercial SD memory card in L series logging function
- Difference between L02CPU-P and L02CPU
- Turning OFF the power with the battery error occurring
- TCP retransmission timer setting for built-in Ethernet port LCPU
- LCPU built-in Ethernet port setting when using the simple PLC communication function