Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22759
  • Release Date : 2018/09/03 17:30
  • Print

Connection status detection between a hub and the built-in Ethernet port of LCPU

Is there any method to know the connection status between the built-in Ethernet port in the L series CPU and a hub?
Category : 

Answer

The bit 10 of the special register SD1288 provides the connection status to a hub. When the bit 10 of SD1288 is ON, a hub is connected.
Product Name
MELSEC-L Series
Series
L Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries